Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21254
  • Release Date : 2018/08/22 16:26
  • Print

Replacement

When replacing the FR-E500 with FR-D700, which parameter numbers of the FR-D700 correspond to Pr.38 (Frequency at 5 V (10 V) input) and Pr.39 (Frequency at 20 mA input) of the FR-E500?
Category : 

Answer

Pr.38 of the E500 corresponds to Pr.125 (Terminal 2 frequency setting gain frequency) of D700. Pr.39 of the E500 corresponds to Pr.126 (Terminal 4 frequency setting gain frequency) of D700.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-D700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries