FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Replacement
FAQ
Replacement
When replacing the FR-E500 with FR-D700, which parameter numbers of the FR-D700 correspond to Pr.38 (Frequency at 5 V (10 V) input) and Pr.39 (Frequency at 20 mA input) of the FR-E500?
- Category :
Answer
Pr.38 of the E500 corresponds to Pr.125 (Terminal 2 frequency setting gain frequency) of D700. Pr.39 of the E500 corresponds to Pr.126 (Terminal 4 frequency setting gain frequency) of D700.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-D700