FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > PS display
FAQ
PS display
In the External operation mode, "PS" is displayed on the operation panel and operation is disabled. What should I do?
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
"PS" is displayed when the inverter is stopped with the "STOP/RESET" button from PU. The PU stop (PS) release method is as follows.
(1) Release method using the operation panel (FR-DU07)
1) After completion of deceleration stop, turn OFF the STF or STR signal.
2) Check the following since the release method depends on the setting value of Pr.79.
- When Pr.79 (Operation mode selection) is "0, 6", PU stop is released by pressing "PU/EXIT" three times.
- When Pr.79 (Operation mode selection) is "2, 3, 7", PU stop is released by pressing "PU/EXIT" one time.
(2) Release method using the parameter unit (FR-PU04/FR-PU07)
1) After completion of deceleration stop, turn OFF the STF or STR signal.
2) PU stop is released by pressing "EXIT".
(3) PU stop is released by resetting the power supply or resetting with the RES signal.
(1) Release method using the operation panel (FR-DU07)
1) After completion of deceleration stop, turn OFF the STF or STR signal.
2) Check the following since the release method depends on the setting value of Pr.79.
- When Pr.79 (Operation mode selection) is "0, 6", PU stop is released by pressing "PU/EXIT" three times.
- When Pr.79 (Operation mode selection) is "2, 3, 7", PU stop is released by pressing "PU/EXIT" one time.
(2) Release method using the parameter unit (FR-PU04/FR-PU07)
1) After completion of deceleration stop, turn OFF the STF or STR signal.
2) PU stop is released by pressing "EXIT".
(3) PU stop is released by resetting the power supply or resetting with the RES signal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700