FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Speed command
FAQ
Speed command
When analog input is used for the speed command, the motor is driven because a little voltage is output with the potentiometer set to 0.
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
Calibrate the terminal 2 bias.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700