FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Switching between External operation mode and PU operation mode
FAQ
Switching between External operation mode and PU operation mode
I want to switch the External operation mode and PU operation mode with the switch.
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
Assign X16 signal, and set Pr.79 to "0", to switch the operation mode with turning ON/OFF X16 signal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700