FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Auto tuning
FAQ
Auto tuning
After performing auto tuning, can I copy the motor constant in the setting value to another inverter and connect the same motor?
- Category :
Answer
Normally, the auto tuning condition depends on the combination of the inverter and motor (including wiring to the motor), perform auto tuning each time.
The parameter required for auto tuning can be used as is.
The parameter required for auto tuning can be used as is.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700