FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Auto tuning
FAQ
Auto tuning
Even though auto tuning is performed, the monitor indicator remains as "1" and RUN LED blinks. What are the possible causes?
- Category :
Answer
With the monitor indicator "1", there is no problem with the parameter setting of auto tuning.
Check if the terminals MRS and SD are not shortened in the wiring of the inverter.
(Check if the signal to externally stop the operation is not input.)
Check if the terminals MRS and SD are not shortened in the wiring of the inverter.
(Check if the signal to externally stop the operation is not input.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700