FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Parameter copy of FR-Configurator
FAQ
Parameter copy of FR-Configurator
Can I save the parameter and copy it to three inverters at the same time with FR-Configurator (FR-SW3-SETUP-WJ)?
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
The parameter can be copied to only one inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700