FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > FR-E710W
FAQ
FR-E710W
Is the FR-E700 with single-phase 100 V input available?
- Category :
Answer
Yes. The model is FR-E710W.
The input is single-phase 100 V, but the output is three-phase 200 V.
The input is single-phase 100 V, but the output is three-phase 200 V.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700