FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Brake unit
FAQ
Brake unit
I want to install an optional brake unit. Although it is described that resistors cannot be used in combination other than described in the instruction manual, can I use the resistors of 200 ? 15 W?
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
The resistors cannot be used in combination other than described.
Operations of brake units and inverters are not verified.
When resistors are used in uncertified combination, the current will be the same if the resistance value is the same, but operations cannot be guaranteed because how long they can be used with a certain current is unknown.
(Do not use the resistor simply by adding the resistance value and wattage.)
Operations of brake units and inverters are not verified.
When resistors are used in uncertified combination, the current will be the same if the resistance value is the same, but operations cannot be guaranteed because how long they can be used with a certain current is unknown.
(Do not use the resistor simply by adding the resistance value and wattage.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700