Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21333
  • Release Date : 2018/08/22 16:27
  • Print

Brake resistor

Which terminal should be connected with the brake resistor? Should I remove the jumper of the terminals P and P1?
Category : 

Answer

Connect the brake resistor to the terminal P and terminal PR. (For the FR-A700-7.5K or lower, remove the jumper of the terminals PR and PX.)
Do not remove the jumper of terminals P and P1. (Remove the jumper of the terminals P and P1 when connecting the power factor improving DC reactor.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries