FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Offline auto tuning
FAQ
Offline auto tuning
The instruction manual describes that "the motor capacity should be equal to or one rank lower than the inverter capacity". When performing offline auto tuning, can I use the inverter with capacity of 1.5K and the motor with capacity of 0.75 kW?
- Category :
Answer
Auto tuning can be performed because the motor is one rank lower than the inverter capacity.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700