FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Faults history
FAQ
Faults history
How should I operate to display the faults history of the inverter?
Is it available during operation?
Is it available during operation?
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
Press the "MODE" key on the operation panel several times to display the faults history screen "E---".
Then turn the setting dial to display the error display screen "E.○○○". Up to eight faults are displayed.
By press the "SET" key in the alarm flashing screen "E.○○○", the output frequency, output current, output voltage, and energization time (0.001 = 1 Hr) can be checked.
They can be checked during operation.
Then turn the setting dial to display the error display screen "E.○○○". Up to eight faults are displayed.
By press the "SET" key in the alarm flashing screen "E.○○○", the output frequency, output current, output voltage, and energization time (0.001 = 1 Hr) can be checked.
They can be checked during operation.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700