FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-PA07
FAQ
FR-PA07
Can I perform the forward rotation and reverse rotation by pressing the FWD/REV key on the enclosure surface operation panel FR-PA07?
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
The forward rotation and reverse rotation are enabled by pressing the FWD/REV key on the operation panel.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700