Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21369
  • Release Date : 2018/08/22 16:27
  • Print

Vector control of the inverter

Under Advanced magnetic flux vector control, what happens with the speed fluctuation ratio with/without encoder?
Category : 

Answer

The speed fluctuation ratio under Advanced magnetic flux vector control of the FR-A500 is as follows.
Without encoder: ±1% With encoder (with A5AP): ±0. 02 % (at power driving load)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries