Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21373
  • Release Date : 2018/08/22 16:27
  • Print

Monitor

Which current and voltage of the phase (maximum value, average value, etc.) are displayed on the operation panel monitor?
Down to two decimal point is displayed for the current. How accurate is this value?
Category : 

Answer

The output current monitor of the inverter displays the output current effective value of the three phases measured by the current sensor.
It does not display the current value of the specific phase.
The output voltage monitor displays the output voltage target value (effective value) of the inverter, and it is not the actual measured value.
For the second digit after the decimal displayed on the output current monitor of the inverter, the accuracy is approximately 90 %.
Product Name
Inverter, magnet motor drive
Series
FR-E500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries