FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500 > Operation of the motor with a brake
FAQ
Operation of the motor with a brake
When using the motor with a brake, I want to operate the brake when the motor stopped completely. Can I detect the motor stop and send the signal to the brake from the inverter?
If it cannot be performed from the inverter, how is the brake operation timing is determined?
If it cannot be performed from the inverter, how is the brake operation timing is determined?
- Category :
Answer
For the general-purpose inverter, the motor stop cannot be detected accurately because the actual motor speed from a motor is not input.
In general, the RUN signal (turned OFF when the inverter is stopped) can be used to send a brake signal.
The SU signal is not suitable for the motor stop judgment because it turns OFF when the output frequency is not reached the frequency command.
To detect the motor stop accurately, when using the FR-A500, install the encoder to the motor and use the encoder control option (FR-A5AP) together.
In general, the RUN signal (turned OFF when the inverter is stopped) can be used to send a brake signal.
The SU signal is not suitable for the motor stop judgment because it turns OFF when the output frequency is not reached the frequency command.
To detect the motor stop accurately, when using the FR-A500, install the encoder to the motor and use the encoder control option (FR-A5AP) together.
- Product Name
- Inverter, magnet motor drive
- Series
- FR-A500