FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > Installing reactor for suppressing harmonics
FAQ
Installing reactor for suppressing harmonics
The catalog explains that one reactor needs to be installed on each inverter. Is it possible to install a reactor on one inverter and connect multiple inverters to the first inverter's output side?
If it is possible, does this configuration conform to the harmonic suppression guidelines for household appliances and general-purpose products?
If it is possible, does this configuration conform to the harmonic suppression guidelines for household appliances and general-purpose products?
- Category :
Answer
You can connect multiple inverters to a single reactor.
In this case, the load seems to be light from the reactor unless all of the inverters are rotating and the power factor improving effect is lowered.
It cannot be judged whether or not this configuration conforms to the harmonic suppression guidelines for household appliances and general-purpose products because this configuration is not covered. However, as mentioned above, the power factor improving effect (harmonics reduction effect) can be obtained as described in catalog when all inverters are operating, this configuration is considered to be acceptable.
In this case, the load seems to be light from the reactor unless all of the inverters are rotating and the power factor improving effect is lowered.
It cannot be judged whether or not this configuration conforms to the harmonic suppression guidelines for household appliances and general-purpose products because this configuration is not covered. However, as mentioned above, the power factor improving effect (harmonics reduction effect) can be obtained as described in catalog when all inverters are operating, this configuration is considered to be acceptable.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Power factor improving reactor
- Series
- Option