FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > Built-in reactor
FAQ
Built-in reactor
Why is it necessary to build in the reactor?
Are the specifications of the built-in reactor same as the FR-BAL?
Are the specifications of the built-in reactor same as the FR-BAL?
- Category :
Answer
The reactor built in the FREQROL-A201 series is intended to stabilize operation of the converter circuit and differs from the FR-BAL. Note that when performing calculations given in the harmonic suppression guidelines, use the conversion coefficient of K31 = 3.4 (no reactor) because the built-in reactor does not have a sufficient harmonic suppression effect.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Power factor improving reactor
- Series
- Option, others