Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21428
  • Release Date : 2018/08/22 16:27
  • Print

Noise from motor at low speed

A high tone noise is heard from the motor when it starts and accelerates to the middle speed.
What are the possible cause and countermeasure?
Category : 

Answer

It is considered to be caused by inverter PWM control.
It can be suppressed by raising the PWM carrier frequency (Pr.72), but the entire noise and leakage current increase.
Adjust the PWM carrier frequency while considering the noise and leakage current.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries