FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500 > Inverter circuit breaker selection
FAQ
Inverter circuit breaker selection
Your catalog of the inverter circuit breakers (NV) shows 200 V, 60 Hz system as a leakage current example of a three-phase motor. Do you also have a 400 V system example?
- Category :
Answer
Since the inverter leakage current is in proportion to the switching voltage of the transistor of the main circuit, the leakage current for the 400 V system is as approximately twice as that of the 200 V system.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- FR-A500