FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Durability in multi-speed setting
FAQ
Durability in multi-speed setting
I want to use the "FR-A520-0.4K" and switch between high-speed operation "55 Hz" and low-speed operation "30 Hz" approximately 20 times per minute.
1. Can I set the minimum acceleration/deceleration time for the above frequency change to an arbitrary value?
2. Does switching speeds too frequently affect endurance?
1. Can I set the minimum acceleration/deceleration time for the above frequency change to an arbitrary value?
2. Does switching speeds too frequently affect endurance?
- Category :
Answer
1. You can set the minimum time by setting the acceleration/deceleration time and acceleration/deceleration reference frequency.
2. No problem with the terminal input. However, you may need a brake resistor depending on the acceleration/deceleration frequency and load condition.
2. No problem with the terminal input. However, you may need a brake resistor depending on the acceleration/deceleration frequency and load condition.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500