FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Options > Difference between FR-AU01 and AU01A
FAQ
Difference between FR-AU01 and AU01A
What is the difference between the FR-AU01 and FR-AU01A?
Do you have material for the FR-AU01A (outline dimensions and specifications)?
Do you have material for the FR-AU01A (outline dimensions and specifications)?
- Category :
Answer
The major changes from FR-AU01 to FR-AU01A include 1. Case material and 2. Lead wire terminal process method.
The FR-AU01A has a backward compatibility with the FR-AU01 and can be used with the FR-Z220-0.4 to 11k.
For details, refer to the following: Figure 1
The FR-AU01A has a backward compatibility with the FR-AU01 and can be used with the FR-Z220-0.4 to 11k.
For details, refer to the following: Figure 1
- Product Name
- Inverter, magnet motor drive
- Product Category
- Manual Controller/Speed controller
- Series
- Option