Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21496
  • Release Date : 2018/08/22 16:27
  • Print

Motor heat generation at low-speed operation

On the A500 series catalog for the FR-A540-3.7K, it is mentioned that continuous operation under 100% torque is possible up to 3 Hz with a constant-torque motor. In the SF-JRCA specifications, 3.7 kW is subject to totally enclosed fan-cooled operation.
Does this mean that operating the SF-JRCA 3.7 kW motor at 3 Hz continuously does not cause a heat generation problem?
Or, does the catalog just mention the standard specifications of the SF-JRCA and is it necessary to provide a specially ordered forced cooling fan when actually operating the motor continuously at 3 Hz?
Category : 

Answer

When using the FR-A540-3.7K in Advanced magnetic flux vector control, operating the motor continuously under the 100% torque at up to 3 Hz does not cause a heat generation problem.

You do not need to provide a specially ordered forced cooling fan.
Note that the 400 V specifications product of the SF-JRCA is a dedicated motor.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries