FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500 > CC-Link
FAQ
CC-Link
When CC-Link is used with inverters FREQROL-V200 and others, is the following communication possible between the inverter and PLC?
1. Input the forward and reverse rotation commands from the hardware terminals and send information of, for example, inverter faulty or operating, from the inverter to PLC via CC-Link.
2. Can I vary the speed commands (running frequency commands) continuously via CC-Link? (I want to accelerate and decelerate the motor from the programmable controller.) If it is not possible to vary the speed commands in 20 msec cycles, should I supply the 0 to 10 V terminal block with voltage?
3. Article (3) on Page 14 of the manual (FR-A5NC)explains "To change the frequency consecutively, be sure to write data to the inverter RAM". What does this mean?
1. Input the forward and reverse rotation commands from the hardware terminals and send information of, for example, inverter faulty or operating, from the inverter to PLC via CC-Link.
2. Can I vary the speed commands (running frequency commands) continuously via CC-Link? (I want to accelerate and decelerate the motor from the programmable controller.) If it is not possible to vary the speed commands in 20 msec cycles, should I supply the 0 to 10 V terminal block with voltage?
3. Article (3) on Page 14 of the manual (FR-A5NC)explains "To change the frequency consecutively, be sure to write data to the inverter RAM". What does this mean?
- Category :
Answer
Although you specify the FR-V200 and others as the inverter models, CC-Link is currently supported by the FR-A500 and FR-E500.
The FR-V200E does not support CC-Link.
1. Yes.
Information on inverter status (for example, faulty, operating status) can be sent via communication in any operation mode.
Also, by setting operation command source (Pr.338) to "1" at the PC link operation mode, you can set the frequency via CC-Link and input the start command from the external terminal.
2. You can vary the speed commands continuously via CC-Link.
The response time is approximately "Sequence scan time + Link scan time × 3 + Inverter processing time of 20 to 30 ms".
For the link scan time, refer to Section 5.2 of the CC-Link System Master/Local Station User's Manual. (It depends on the number of inverters connected, baud rate, and other factors.)
The response time for 0 to 10 V input is approximately 100 ms (initial setting).
Therefore, varying the speed commands in 20 ms cycle as you requested may not be addressed.
3. The inverter frequency is set by the instruction code written in the EEPROM and RAM (HEE) and by the instruction code written in the RAM only (HED).
The EEPROM is mainly used to memorize the setting frequency and the RAM is used to store the frequency used for actual operation of the inverter.
Since the EEPROM has the life for data writing, frequency writing to the EEPROM may damage it. Therefore, if you are changing the setting frequency frequently, use the instruction code written in the RAM only (HED).
The FR-V200E does not support CC-Link.
1. Yes.
Information on inverter status (for example, faulty, operating status) can be sent via communication in any operation mode.
Also, by setting operation command source (Pr.338) to "1" at the PC link operation mode, you can set the frequency via CC-Link and input the start command from the external terminal.
2. You can vary the speed commands continuously via CC-Link.
The response time is approximately "Sequence scan time + Link scan time × 3 + Inverter processing time of 20 to 30 ms".
For the link scan time, refer to Section 5.2 of the CC-Link System Master/Local Station User's Manual. (It depends on the number of inverters connected, baud rate, and other factors.)
The response time for 0 to 10 V input is approximately 100 ms (initial setting).
Therefore, varying the speed commands in 20 ms cycle as you requested may not be addressed.
3. The inverter frequency is set by the instruction code written in the EEPROM and RAM (HEE) and by the instruction code written in the RAM only (HED).
The EEPROM is mainly used to memorize the setting frequency and the RAM is used to store the frequency used for actual operation of the inverter.
Since the EEPROM has the life for data writing, frequency writing to the EEPROM may damage it. Therefore, if you are changing the setting frequency frequently, use the instruction code written in the RAM only (HED).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- FR-E500, FR-A500