Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21565
  • Release Date : 2018/08/22 16:28
  • Print

Inverter selection when multiple inverters are to be connected

When multiple inverters are to be connected, how should I choose them?
Category : 

Answer

Be sure to use a high power factor converter with the capacity higher than the total capacity of the inverters connected. (Note: One or more of the inverters must have capacity more than half of the high power factor converter.)
Product Name
Inverter, magnet motor drive
Product Category
High power factor converter
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries