Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21573
  • Release Date : 2018/08/22 16:28
  • Print

Accessories and inverter with built-in high power factor converter

Do you have a product that contains the reactor 1, reactor 2, and outside box in the same case?
Also, do you have an inverter with a built-in high power factor converter?
Category : 

Answer

If the reactor 1, outside box, and reactor 2 are contained in the same case as the high power factor converter, the unit becomes larger and heavier while freedom of arrangement decreases, making it harder to handle the unit. These are provided as accessories for this reason.

We do not have a product with accessories contained in the same case nor an inverter with a built-in high power factor converter.
Product Name
Inverter, magnet motor drive
Product Category
High power factor converter
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries