Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21578
  • Release Date : 2018/08/22 16:28
  • Print

Can a single potentiometer operate two speed controller?

Can a single potentiometer operate two speed controller?
Category : 

Answer

A single potentiometer cannot operate two speed controller.

Reason:
Since the control circuit and main circuit of the SC-A speed controller are not insulated, connecting two speed controllers to a single potentiometer may generate undesirable current that may break the speed controllers.
(You can operate two speed controllers by using an insulated double potentiometer.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter speed controller
Series
SC-A

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries