FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > What parameters (settings) are available?
FAQ
What parameters (settings) are available?
What parameters (settings) are available?
- Category :
Answer
The following three functions can be set:
- Acceleration/deceleration time- Electronic thermal O/L relay- Maximum frequencyThe parameter unit is not used but two internal potentiometers and two switches are used for setting.
- Acceleration/deceleration time- Electronic thermal O/L relay- Maximum frequencyThe parameter unit is not used but two internal potentiometers and two switches are used for setting.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter speed controller
- Series
- SC-A