FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-U100 > What are the specifications of totally enclosed type?
FAQ
What are the specifications of totally enclosed type?
What are the specifications of the totally enclosed type?
- Category :
Answer
The totally enclosed type is JEM1030 IP40.
(IP40: Structure that prevents the tip of a solid object exceeding 1 mm in diameter or thickness (wire or steel belt) from entering the inside)Be sure to use it in the surrounding air temperature of -10 to + 40 deg C.
(IP40: Structure that prevents the tip of a solid object exceeding 1 mm in diameter or thickness (wire or steel belt) from entering the inside)Be sure to use it in the surrounding air temperature of -10 to + 40 deg C.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Common
- Series
- FR-U100