FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Can I use digital operation panel FR-DU01?
FAQ
Can I use digital operation panel FR-DU01?
Can I use the digital operation panel FR-DU01?
- Category :
Answer
You cannot use it with the standard and multi-function products.
It can be connected to the dedicated PU operation type only. (Note that the FR-DU01 is an operation-only unit and you cannot set parameters with it.)
It can be connected to the dedicated PU operation type only. (Note that the FR-DU01 is an operation-only unit and you cannot set parameters with it.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Common
- Series
- FR-U100