FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Types available for FR-AU03
FAQ
Types available for FR-AU03
Can I use the FR-AU03 with the FR-A200, FR-Z, and FR-U series?
- Category :
Answer
The FR-AU03 is a dedicated product for the FR-A024.
Although it cannot be attached directly to other inverters (FR-A200 and FR-Z, FR-U series), it can be used as a separately installed operation panel using the optional cable FR-CBL.
Although it cannot be attached directly to other inverters (FR-A200 and FR-Z, FR-U series), it can be used as a separately installed operation panel using the optional cable FR-CBL.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024