Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21634
  • Release Date : 2018/08/22 16:28
  • Print

Plug-in options

Can I use the plug-in option used with the FR-A200 with the FR-A200EXCELLENT?
Category : 

Answer

Use the plug-in option dedicated for the FR-A200EXECLLENT.
The plug-in option for the FR-A200EXECLLENT cannot be used with the FR-A200.
To avoid installing an incorrect plug-in option, the connector position of the option for the FR-A200EXCELLENT is different from the option for the FR-A200.
Do not install an incorrect option forcibly because doing so breaks the plug-in option unit.

The functions of the FR-EPA to FR-EPE are the same as those of the conventional FR-A200 options (FR-APA to FR-APE).
For the FR-A200EXCELLENT, the FR-EPG and FR-EPH options are added.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
FR-A200

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries