Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21641
  • Release Date : 2018/08/22 16:28
  • Print

Motor wiring length

How far apart can the vector inverter and motor be?
Category : 

Answer

Up to 50 m. Be sure to connect the encoder cables in parallel and use the thicker cable gauge.
You can extend this distance up to 100 m by using the long distance cable power supply that is a plug-in option.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries