Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21660
  • Release Date : 2018/08/22 16:28
  • Print

New function of EXCELLENT

What are the new function of the A100E compared with the A100?
Category : 

Answer

The new function includes:
- PI control function
- Cumulative energy monitor (monitor accuracy: approximately ±25% of full scale value)
- Response current limit operation is improved.
- Extended carrier frequency setting range (0.7 to 14.5 kHz)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A100

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries