Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21683
  • Release Date : 2018/08/22 16:28
  • Print

Frequency setting

As Pr.7 (Acceleration time) and Pr.8 (Deceleration time) set time to accelerate the frequency to the value set by Pr.20 (Acceleration/deceleration reference frequency), the maximum frequency I need is just 20 Hz.
Can I set Pr.20 to 20 Hz?
Category : 

Answer

Yes, you can set Pr.20 to 20 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries