Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21710
  • Release Date : 2018/08/22 16:29
  • Print

FR-Configurator

Can I connect a single instance of the FR-Configurator (FR-SW3-SETUP-WJ) setup software to multiple inverters via USB?
Category : 

Answer

No. You cannot connect it to multiple inverters.
You can only connect a single personal computer to a single inverter via USB.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?