FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > FR-Configurator
FAQ
FR-Configurator
While using the inverter's terminal 4 (for 4-20 mA) and supplying 20 mA, I want to operate it at 85 Hz.
Can I set this by using the optional setup software (FR-SW3-SETUP-WJ)?
Can I set this by using the optional setup software (FR-SW3-SETUP-WJ)?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Yes, you can use the setup software (FR-SW3-SETUP-WJ) to set it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700