FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Monitor indicator
FAQ
Monitor indicator
I set the rotations per minute to Pr.37 (Speed display). Can I check the accumulated number of rotations on the monitor?
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
No. You cannot check the accumulated number of rotations on the monitor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700