Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21729
  • Release Date : 2018/08/22 16:29
  • Print

Operation panel (FR-PA02)

When using the operation panel (FR-PA02) for FR-E500 with other inverters, how should I set Pr.146 (Built-in potentiometer switching)?
Category : 

Answer

Set Pr.146 (Built-in potentiometer switching) to "0".
This allows for using the potentiometer built in the FR-PA02 to set the frequency.
(Set this parameter to "1" when the built-in potentiometer is not used.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries