Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21735
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

Do I have to press the "SET" key when setting the frequency with the setting dial?  
Category : 

Answer

You need to press the "SET" key with the initial setting.

The frequency is not set unless you press the "SET" key.

Setting Pr.161 (Frequency setting/key lock operation selection) to "1" activates the potentiometer mode and the inverter operates at the frequency set by the setting dial without pressing the "SET" key.
(The frequency setting value is memorized in approximately 10 seconds after it becomes stable after being set by the setting dial.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries