FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Advanced magnetic flux vector control
FAQ
Advanced magnetic flux vector control
To perform Advanced magnetic flux vector control, I set Pr.71 (Applied motor) to "3", Pr.80 (Motor capacity) to "0.75 K", Pr.83 (Motor rated voltage) to "200 V", Pr.84 (Rated motor frequency) to "60", and Pr.96 (Auto tuning setting/status) to "1", but "1" is not shown when the screen returned to the monitor window.
What is wrong?
What is wrong?
- Category :
Answer
Check the parameters necessary for tuning again.
Check if Pr.9 (Electronic thermal O/L relay) and Pr.81 (Number of motor poles) are set correctly.
Check if Pr.9 (Electronic thermal O/L relay) and Pr.81 (Number of motor poles) are set correctly.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700