FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Monitor indicator
FAQ
Monitor indicator
How can I switch the monitor display from the output frequency to output current?
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
Press the "SET" key once while the output frequency is monitored.
The unit indicator LED changes from "Hz" to "A" and the monitor display changes to the current.
The unit indicator LED changes from "Hz" to "A" and the monitor display changes to the current.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700