FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Terminal setting
FAQ
Terminal setting
I want to use the terminal 4 of the inverter as the voltage input terminal. How should I configure the setting?
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
To use the terminal as voltage input, you need to:
- Set Pr.267 (Terminal 4 input selection).
- Set the voltage/current input switch on the inverter board.
- Set the short-circuit of the terminals AU and SD.
Pr.267 selects the input voltage from 0 to 5 V and 0 to 10 V.
Set the switch to the "V" (voltage) side.
Assign the terminal AU (Terminal 4 input selection) to an unused terminal.
- Set Pr.267 (Terminal 4 input selection).
- Set the voltage/current input switch on the inverter board.
- Set the short-circuit of the terminals AU and SD.
Pr.267 selects the input voltage from 0 to 5 V and 0 to 10 V.
Set the switch to the "V" (voltage) side.
Assign the terminal AU (Terminal 4 input selection) to an unused terminal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700