FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Minimum frequency
FAQ
Minimum frequency
When the minimum frequency is set to 3 Hz, how does the inverter operate?
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
If any other frequency is not set, when the start signal is input, the inverter starts acceleration from 0.5 Hz set with Pr.13 (Starting frequency) up to 3 Hz in accordance with the acceleration time.
The inverter cannot operate at frequencies lower than 3 Hz even if the frequency is set.
The inverter cannot operate at frequencies lower than 3 Hz even if the frequency is set.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700