Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21780
  • Release Date : 2018/08/22 16:29
  • Print

Output voltage

I checked the U, V, and W output voltages using a tester and the measured voltages were just 15 V while the output frequency had been increased.
Is this a failure?
Category : 

Answer

Since the output frequency was measured, it is considered that the start signal was input correctly.

Check the output voltage on the voltage monitor of the inverter.

The output voltage of the inverter becomes low when the output frequency is low.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries