FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Setting frequency
FAQ
Setting frequency
When using the inverter in the external operation mode, the frequency setting value set by the external potentiometer is not output until the inverter operates. Therefore, I cannot confirm while setting it.
I want to check the setting frequency while the inverter is stopped.
I want to check the setting frequency while the inverter is stopped.
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
Set Pr.52 (DU/PU main display data selection) to "100".
Displaying the setting frequency while the inverter is stopped and the output frequency while it is operating on the monitor.
Displaying the setting frequency while the inverter is stopped and the output frequency while it is operating on the monitor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700