Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21786
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

If I set Pr.77 (Parameter write selection) to "2", can I use the setting dial to set the frequency even during operation?  
Category : 

Answer

You can use the setting dial to set the frequency during operation even if Pr.77 is not set to "2".
Setting Pr.77 to "2" allows for changing the parameter settings during operation.
With the initial setting, you need to turn the setting dial to select frequency and press the "SET" key to accept it.
Setting Pr.161 (Frequency setting/key lock operation selection) to "1" allows for using the setting dial as a potentiometer.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries