Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21829
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

I perform CC-Link operation. While Pr.544 (CC-Link extended setting) is set to "12" for double setting, should I set it to quadruple setting to check the fault records?  
Category : 

Answer

You can check the fault records with Pr.544 (CC-Link extended setting) set to "12" for double setting.
Set H74 for the instruction code and turn ON RYF.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries