FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > CC-Link
FAQ
CC-Link
In CC-Link operation, when I powered ON the inverter with Pr.79 (Operation mode) set to "2" and Pr.340 (Communication startup mode selection) set to "10", the CC-Link NET operation mode was activated and the NET LED turned on.
I set Pr.543 (Baud rate selection) to "2" but the inverter does not operate with the RUN LED blinking.
I powered OFF and then ON again the inverter and it did not operate.
What is the cause of this?
I set Pr.543 (Baud rate selection) to "2" but the inverter does not operate with the RUN LED blinking.
I powered OFF and then ON again the inverter and it did not operate.
What is the cause of this?
- Category :
Answer
Check if the master station uses CC-Link Version 1 and the FR-A7NC uses CC-Link Version 2.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700